STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1591 Views
  • 0 replies
  • 2 kudos

X-NUCLEO-GFX02Z1 with Nucleo-H755ZI-Q X-Cube Display Package

In the X-Cube Display Package there is a HelloWorld Application for X-NUCLEO-GFX02Z1 with a NUCLEO-H723ZG. Is it possible to change it in a way to make it on Nucleo-H755ZI-Q running?Otherwise, is there a step by step manual to get the display X-NUCLE...

guc by Associate II
  • 4718 Views
  • 8 replies
  • 0 kudos

My own Visual "Configurator"

Hi guys!Still live and kicking, thanks God! My fist public version was/is vscode_nucelo_l152re (totally uninspired, I am bad with naming things) that is a visual configuration tool for the Nucleo_L152RE board and generates code that uses the old SPL ...

Resolved! Did CubeMX 6.7 break H7 Clock Configuration?

Hi,I have just updated to CubeMx 6.7 and now my stm32H755 nucleo board shows error while setting to 480MHz. I'm pretty sure that this board can run this fast before.Did the new CubeMx break clock config feature for H7 devices? There is also this craz...

0693W00000WJnaxQAD.png 0693W00000WJnbgQAD.png
HHuyn.15 by Associate II
  • 4404 Views
  • 4 replies
  • 0 kudos

Resolved! CubeIDe 1.15.0 FW_f4_1.28.0 USB CDC not working

Hello, I have a very simple code written with earlier versions of CubeIDE and FW_F4_1.26.2 for STM32F405rgt6It is a very simple code, just sending a message via USB as a CDC Device . If I download the old .elf file to controller, everything works fin...

RÖztü.1 by Associate II
  • 3470 Views
  • 2 replies
  • 1 kudos

The CubeMX/CubeIDE login issue is resolved

Hello CubeMX/CubeIDE users.  From the time period of May 14 to May 17, 2024, some users have faced issues when connecting to the ST network while using CubeMX or CubeIDE.Some examples were issues downloading firmware packages using STM32CubeMX and ST...

stm32l010f4p6 not work with MSI clock 32.768khz

"I am setting up the clock for 32.768kHz, but when I compile and test it, it doesn't work. I place a simple counter in the while loop, but it doesn't increment."i have in the while a counter, but not increment. 

clock.JPG
jdo by Associate II
  • 2300 Views
  • 3 replies
  • 0 kudos

Resolved! True version number for the CMSIS-RTOS ("injected" by CubeMX)

Hi all!Where do I find the "true" version number for the CMSIS-RTOS code "injected" by CubeMX?While STM32CubeMX (v6.9.1) shows "2.0.0"..... the header file in my project (CMSIS_RTOS_V2/cmsis_os.h) has the following in the comment header* $Date: 10. J...

mwb_0-1715758081462.png
mwb by Associate III
  • 1948 Views
  • 1 replies
  • 1 kudos