STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1560 Views
  • 0 replies
  • 2 kudos

Resolved! STPackCreator Global/Project define.

Hi all.Working with the Pack Creator I know I can create a header file that contains defines that are editable in the CubeMX view.I'd like to know if it's possible to have a pack that places defines in the project settings instead of a header file? 

pywtk by Associate II
  • 1958 Views
  • 3 replies
  • 0 kudos

STPackCreator with H5 Discovery Kit

Hi all!I'm creating a pack using the Pack Creator. My pack uses a BSP template. I've tried creating projects using the pack for a selection of boards. In all cases bar the H5 the pack template successfully creates the right #include for the platform ...

pywtk by Associate II
  • 997 Views
  • 0 replies
  • 1 kudos

Twice used Pin Lables in CubeMX

Hello,because of my mistake, I had assigned the same label for two different pins within CubeMX 6.12. It seems, CubeMX recognize this, but send not an error oder a warning message about it. What happen, CubeMX is attaching the port- and pinname to th...

JPiet.3 by Associate III
  • 1594 Views
  • 1 replies
  • 1 kudos

Resolved! Flash memory - STM32F030C8 Erase Cycles

Hello I'm using STM32F030C8.I'm writing the code because I want to use the internal flash memory like rom.Is there a set number of times I can write in internal flash memory? If there is a related document, I would like to see it.Thank you.

giwonKIM by Associate III
  • 2104 Views
  • 5 replies
  • 3 kudos

Resolved! the Pinout and Configuration .ioc is wrong

I have been using STM32F767zi for long time.I know some of the pin feature by heart.Last night, I enabled ETH for a moment and to see what pin it uses, then I disable it and then all the chaos happened.I realized that many of frequently used USART 2,...

Wai Siang by Associate III
  • 3865 Views
  • 2 replies
  • 1 kudos

Resolved! Why is I2S Frequency in Clock Configuration so high?

Hi STM community!I am new to STM microcontrollers and this is my first post :)My board is a tiny STM42F401CCU6 @ 84MHz. I already have made some first steps with CubeMX and CubeIDE, after I came from the arduino IDE which was a bit too simple (readin...

Stipe_0-1721847172491.png
Stipe by Associate II
  • 2757 Views
  • 1 replies
  • 3 kudos

Resolved! STPackCreator Insert Code Snippets into main.c

Hi all!Thanks again for the help so far.Just another question, is it possible (or normal?) when creating a pack to have it insert snippets of code into main.c just like the code snippets that get inserted by the cube when you change peripherals etc? ...

pywtk by Associate II
  • 1249 Views
  • 1 replies
  • 0 kudos