STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1557 Views
  • 0 replies
  • 2 kudos

Resolved! Device Configuration Tool does not generate the code.

I have been using STM32CubeIDE (Version: 1.10.1) with STM32CubeMX - STM32 Device Configuration Tool Version: 6.6.1-RC2.But when i do some modification in device configuration and then try to generate the code , it does not generate the code. But when...

KKato.2 by Associate III
  • 27483 Views
  • 14 replies
  • 12 kudos

LWIP DHCP Configuration on CubeMX

 Hi,I am trying to configure DHCP on my STM32F746G-DISCO board, but despite several attempts and even after setting up my DHCP server or configuring my router, I can't get a dynamic IP for my MCU. I can make it work with a static IP, but I would like...

KDZ7 by Associate
  • 3640 Views
  • 2 replies
  • 1 kudos

dac & adc with stm32cubemx and keil

I have a project using nucleo stm32f334.With the way it worksI get the adc value from the 12 bit potentiometer. Then I want to display the value using dac and see the frequency, period and voltage from the oscilloscope.I want the magnitude of the fre...

Resolved! ADC to DAC

hallocan anyone help me about how to program for convert adc to dac ini stm32cubemx with program keil U5, have you guys can help to bring me an example of your code or tips and step. i used the potentiometer for adc value and the value used to dac an...

Resolved! can stm32f103cbt6 usb work under HSI clock?

I use stm32CubeMX to generate usb code with HSI clock.Though I can config with usb clock to 48MHz, But stm32CubeMX software display there is clock issue as below:So I wonder can stm32f103cbt6 usb work under HSI clock? 

shengyang_0-1721886626870.png

IRRemote on STM32L4RI-DISCO

Hi, I'm new to STM32. I have an STM32L4RI-DISCO board and would like to add an IR receiver and decode RC5 signals. According to AN4834, IRTIM can be used on STM32L4. I have downloaded en.x-cube-irremote.zip.Firstly it is not recognized by Cube MX.Sec...

Lanceh by Associate III
  • 2070 Views
  • 3 replies
  • 0 kudos