STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

Resolved! There is no Advanced Parameters tab on the Ethernet

Hello. I'm trying to use Ethernet MAC with external PHY (LAN8720) but when I try to configure the Ethernet on the IOC there is no Advanced Parameters tab (STM32F407VGT6). HAL Lib. version is 1.27.1. I tried a few things but I had no luck. I think I'm...

0693W00000bhMLPQA2.png
MrEmou by Associate II
  • 5033 Views
  • 6 replies
  • 0 kudos

Resolved! ADC dual mode

Hi i'm using MCU : STM32H743ZGT. At several ADC documents, it says that when ADC1 and ADC2 end sampling, the two results are stored in ADC_CDR together. The top 16 bits are the result of ADC2, or slave ADC, and the bottom 16 bits are the result of AD...

giwonKIM by Associate III
  • 2463 Views
  • 3 replies
  • 1 kudos

Resolved! To Generate 2 pwm with phase shift with same timers

 logic analyser picture has timer 1 channel 1 and another one is channel 2 it's duty 30% and frequency 100khz it's total ton+toff is 10 microseconds here I need to start the timer 1 channel 2 after 5 microseconds  I need the output like this I I'm dr...

1000012502.jpg 1000012503.jpg

How to update STM32CubeMX version in CubeIDE?

Hi,i want to import BLE_p2pServer example in CubeIDE 1.16.0 i got the message "This file has been generated with STM32CubeMX version '6.12.1'.Your current STM32CubeMX version is '6.12.0'." When i check for Updates, then I only have the option of upda...

2024-10-10_13h35_10.png 2024-10-10_13h36_10.png
ledi001 by Senior
  • 6810 Views
  • 7 replies
  • 1 kudos

FreeRTOS Middleware can not enable MPU function?

我正在使用STM32L431RCT6,我的 HAL 版本是最后一个。我想使用 FreeRTOS 的最后一个 API 让我的项目更稳定: BaseType_t xTaskGenericNotify( TaskHandle_t xTaskToNotify, uint32_t ulValue, eNotifyAction eAction, uint32_t *pulPreviousNotificationValue ) PRIVILEGED_FUNCTION; #define xTaskNotify(...

Wshuo1_0-1728564635757.png Wshuo1_1-1728564960228.png Wshuo1_2-1728564976868.png Wshuo1_3-1728564986038.png
Wshuo.1 by Associate II
  • 1481 Views
  • 2 replies
  • 1 kudos

Resolved! BSP example code generation issue

Hi,I am currently encountering an issue with STM32CubeMX (v6.12.1) when trying to generate the sample BSP code for the STM32H755ZI-6U (Nucleo-H755ZI-Q development board). Specifically, the usual pop-up prompt to select BSP drivers for demonstration c...

Resolved! help for STM32packcreator

hello, I can not find any good doc for packcreator. I would like to add a folder to my pack, it should be add on the root of my project. it is a tools for win, (exe, py, ...). I have added to others file and as a component. but after generating the p...