cancel
Showing results for 
Search instead for 
Did you mean: 

Can't install new toolchains because of STM32CubeIDE ToolChain Manager Network error Issue

Schmesterle
Associate II

I have installed Version 1.11.0 from STM32CubeIDE and have to install an older toolchain for my stm32H7 project. But Toolchain Manager throws the error "Failed to fetch the toolchain list, please check your network settings."

In the thread behind this link Employee Julien D say that this is a known error, but in my case I'm not able to choose a new toolchain.

Is there a workaround for this problem?

1 ACCEPTED SOLUTION

Accepted Solutions
Julien D
ST Employee

Because of bigger troubles occurring when installing additional features we took the decision to disable temporarily our repository. See https://community.st.com/s/question/0D53W00001zeSZcSAM/stm32cubeide-intool-update-issue

The main reason is that it could break your STM32CubeIDE installation, such in a unrecoverable state.

A fix should be deployed soon.

Apologize for the inconvenience.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Julien D
ST Employee

Because of bigger troubles occurring when installing additional features we took the decision to disable temporarily our repository. See https://community.st.com/s/question/0D53W00001zeSZcSAM/stm32cubeide-intool-update-issue

The main reason is that it could break your STM32CubeIDE installation, such in a unrecoverable state.

A fix should be deployed soon.

Apologize for the inconvenience.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Schmesterle
Associate II

Thank you for your answer.

Searching for release notes brings up an 1.11.2 where this issue is adressed.

https://www.st.com/resource/en/release_note/rn0114-stm32cubeide-release-v1110-stmicroelectronics.pdf

I will check when 1.11.2 is released

Edit: Everything works perfect in 1.11.2

adriaan-mernok
Associate II

I am still experiencing this issue with v1.14.0 in 2024.

Resorted to using STM32CubeIDE in Linux via WSL.