STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 USART receiving sting

Posted on September 29, 2016 at 07:07 I started 2 days ago working on STM32f4 discovery board, and i have basic background in C programming. I succedded in sending and receiving characters using USART with interrupt, but whenever i try to re...

Modbus/RTU on STM32F303

Posted on September 16, 2014 at 11:54Hello everyone, i am implementing Modbus/RTU protocol on STM32F303 and i want to check something, because i don't know if i understand this correct. According to RM ModBus/RTU: In this mode, the end of one block ...

usart communication using interrupts

Posted on September 30, 2016 at 09:25Hi everyone! I am doing a project using the HY-MiniSTM32V board.the software used are STM32CubeMX and the IDE is Atollic TrueStudio. I wrote the following code for receiving data back from the terminal(Tera Term)...

anjana087 by Associate II
  • 1664 Views
  • 2 replies
  • 0 kudos

Micro-second delay function for STM32F0 ?

Posted on September 30, 2016 at 18:22Since it seems like the DWT is not available for the F0 series, is the only way is to have a long loop for micro-second delay? For example, if the F0 runs at 48MHz, if I have a loop like this: for (uint32_t idx =...

Vu.Andy by Associate III
  • 1015 Views
  • 3 replies
  • 0 kudos

RTC random interrupt

Posted on September 30, 2016 at 18:22HelloI have 2 PCB with STM32L476. The same code is running on each PCB (both board have been programmed with the STlink-utility and the same binary file). The RTC is configured to provide a 1Hz IRQ. The RTC clock...

0690X00000605S4QAI.png
tarzan2 by Senior
  • 780 Views
  • 1 replies
  • 0 kudos

NUCLEO-F746, DAC circular DMA bug!

Posted on September 30, 2016 at 18:28&sharpdefine SAMPLESDAC (1024*2)static TIM_HandleTypeDef  Timer4Handle;void Timer4_init(){    TIM_ClockConfigTypeDef TimerClockConfig;    TIM_MasterConfigTypeDef sMasterConfig;    __TIM4_CLK_ENABLE();    //Timer ...

kylongmu by Associate II
  • 1794 Views
  • 5 replies
  • 0 kudos

HAL Bug Report - F4xx, Timer Complimentary Outputs

Posted on September 22, 2016 at 16:11Using latest CubeMX and HAL libs.As far as i can see, HAL doesn't support a method for enabling the TIMx complimentary CHxN outputs.In this case i want to use TIM1 CH1N and CH2N for PWM output.Thanks.

mwp by Senior
  • 2292 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.