STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1570 Views
  • 0 replies
  • 2 kudos

Problem with CubeMX 4.5.0 with Linux

Posted on January 12, 2015 at 11:38Hello all. Bed path: java.io.FileNotFoundException: /home/krzysiek/STMicroelectronics/STM32Cube/STM32CubeMX/db/plugins/projectmanager\stm32tck.cfg (No such file or directory) at java.io.FileInputStream.open(Nativ...

giver3 by Associate II
  • 1197 Views
  • 2 replies
  • 0 kudos

LWIP process call frequency

Posted on February 04, 2016 at 11:25Hi all, Quite new in the development with LWIP, there is a question I have not found any answer so far; What is the minimum / maximuum frequency at which the main LWIP process function shall be called? I'm talking...

STM32CubeMX annoying behaviour

Posted on February 05, 2016 at 13:01Hi, I am using the current version (4.12.0) of STM32Cube. Every time I open a *.ioc file, it is immediately regarded as changed -- it's marked by a star in the window title and if I want to exit, I get a warning ...

zabel by Associate III
  • 801 Views
  • 0 replies
  • 0 kudos

STm32CubeMx Generated Code w/ RTOS for EWARM toolchain

Posted on January 28, 2016 at 22:18I used Stm32CubeMx with STM32Cube_FW_F0_V1.4.0 to generate my project on STM32F030CC with FreeRTOS and EWARM toolchain. In debug mode. I only have the generated code at this time. It first crashes on HAL_TIM_PWM_Co...

fsavaria by Associate II
  • 986 Views
  • 1 replies
  • 0 kudos

STM32CubeMX not running

Posted on January 14, 2016 at 09:55My installation of STM32CubeMX is not working. I tried to reinstall the application but the Windows Control Panel -> Programs and Features Uninstall function does not work. I deleted the installation directory manu...

0690X00000604lBQAQ.png

CubeMX F3 bug

Posted on January 23, 2016 at 15:27CubeMX: 4.12.0STM32Cube_FW: F3_V1.2.0MCU: Stm32F303VCT(stm32-f3-discovery)I configure OPAM4 to ''PGA not connected'', Non-inverting input is configured to PB11.Cube generates code:  hopamp4.Init.NonInvertingInput =...

elijah by Associate III
  • 1112 Views
  • 1 replies
  • 0 kudos

Strange output in STM32CubeMX Ver 4.12.0

Posted on January 22, 2016 at 22:09I recently upgrade CubeMX to version 4.12.0 and used it to generate code for a custom STM32F407VGT board. Everything seemed to work fine with previous versions, but not so much with the latest version. For example....

AN for runtime RAM/Stack usage of the STM32 application

Posted on January 21, 2016 at 17:20HI, Is there any Application Note for runtime stack and RAM utilization of the STM32 application .Any tool specific to Nucleo for evaluating the application?Is STM Studio meant for that?Rgds,R #!stm32-!cubemx #s...

darla14 by Senior
  • 1857 Views
  • 3 replies
  • 0 kudos