STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

STM32CubeMX and F1 package v1.3

Posted on January 03, 2016 at 13:40I have STM32CubeMX v4.12, Check for Updates revealed STM32CubeF1 Release 1.3 After dondloadint , but Cube say: This Package version is not managed on this version of STM32CubeMX. Wher is probl�m?  I am talkingabout...

asrock70 by Associate II
  • 3559 Views
  • 6 replies
  • 0 kudos

Do I need both STM32CubeMX and STM32CubeF4?

Posted on May 13, 2014 at 04:41HelloI'm new with ST microcontrollers and reading the documentation I can see that there is STM32CubeMX and STM32CubeF4. I read also that STM32CubeMX contains the STM32CubeF4 or something like that.My question is; If S...

m4l490n by Senior
  • 3132 Views
  • 8 replies
  • 0 kudos

STM32CubeMX data model

Posted on December 01, 2015 at 12:41Hi, The STM32CubeMX data model is mentioned in the user manual UM1718, I'd like to use some more advanced custom code generation but am getting stopped by a lack of spec for the data model. Is the data model speci...

guy2399 by Associate
  • 1060 Views
  • 1 replies
  • 0 kudos

STM32CubeMX F3 Comparator & ADC -- AN4232

Posted on January 10, 2016 at 23:19I am reading through AN4232 on using the F3 comparator and it notes in section 2.3 that the comparator input is also an ADC channel.  I would like to use the channel for both, however I have not found a way in STM3...

STM32CubeMX does not allow setting CRC Polynomial

Posted on September 29, 2015 at 12:22I want to set the CR polynomial according to the most top table in http://users.ece.cmu.edu/~koopman/crc/index.html However STM32CubeMX does not allow to do it due to the following restrictions: ---- CRCPolynomia...

caco3 by Associate II
  • 1006 Views
  • 1 replies
  • 0 kudos

I2S code generated by STM32CubeMX for STM32F746 - no MCKO

Posted on December 12, 2015 at 19:37Hello,I'm using STM32CubeMX to generate a project for STM32F746VGT6.Everything works fine except I2S3, there is no clock output on MCKO pin (PC7) and the call of HAL_I2S_Transmit(...) generates a timeout error.The...

fmcarp by Associate
  • 2008 Views
  • 3 replies
  • 0 kudos

STM32CubeMX work is too slow.

Posted on December 27, 2015 at 19:31STM32CubeMX is very useful program.Only too slow, on my computers.Each click is delaying work on a lot of seconds.My computers use AMD Athlon & E1 processors.This is not enough? What should I do?Everything happens...

CubeMX - STM32F411 code generation CDC ACM bug ?

Posted on December 23, 2015 at 00:00 Hi, not sure it's a bug because it's my first time with CDC ACM. But After a fresh CubeMX generation with USB_OTG_FS in device mode. I just add this : uint8_t buf[] = ''Hello\r\n''...

ziz by Associate II
  • 933 Views
  • 1 replies
  • 0 kudos

CubeMX and FreeRTOS version update

Posted on March 13, 2015 at 16:08Hi,I'm starting 2 new projects (1 with STM32F407 and one with STM32L152).Currently the CubeMX integrates the freeRTOS 8.1.2, when will this be updated to the 8.2?What is the ST strategy regarding the updates?What wou...

daniele by Associate II
  • 2623 Views
  • 4 replies
  • 0 kudos