STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1572 Views
  • 0 replies
  • 2 kudos

How to include codes from examples

Hi,I am using Nucloe144 H743 board, Cube Mx and true studio. I want to incorporate codes given in cubeH7 example for EVal boads. How i can do this? For example how i can use FatFs application Code for EVAL boards in Nucleo or Other Custom boards......

Resolved! STM32CubeMX 5.0.1 No vertical bar for window scrolling

The vertical scroll bar in the GPIO Settings window used in various peripheral does not appear.Left-click on a timer (for example), in the central window you can see the "Configuration -> Parameter Settings" with the vertical scrol bar, this is OK. I...

0690X000006D8q7QAC.jpg 0690X000006D8qCQAS.jpg

How to configure PHY in MII mode using cubeMX?

I want to work on ethernet using MII mode. At times i am getting struck in clock configuration also. In lwip.c file, the link is getting up but while pinging the board from pc am getting destination host unreachable. Please help to resolve the proble...

PSrin by Associate
  • 1926 Views
  • 3 replies
  • 0 kudos

CubeMX: How to DELETE configuration of a peripheral?

Suppose you configure a timer, then decide you don't want that one.How is one supposed to remove it?I've tried delete key, all views, finally edited the IOC file.Really now! This user interface would get us canned if we delivered it to a customer...T...

Sine Pulse Width Modulation using STM32F407VG

Hi all, I am trying to program a Sine PWM using STM32F407VG, but i only got the complementary PWM instead. Can some kind person tell what can i amend or add? attached is my code. I am using ac6 system workbench for coding. Thanks.

jon1280 by Associate
  • 1635 Views
  • 2 replies
  • 0 kudos

STM32CubeMX does not start!

Helloo,Problem occured after updating STM32CubeMX from ver 4.x to ver 5.0.1. It was running perfectly before. But now, when I try to start it, nothing happens acceps my mouse icon turn into spinnnig icon for few seconds.I did try to uninstall STM32Cu...