STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

STM32CubeMX Generating Code with Licensing Issues

When selecting "Makefile" for Toolchain/IDE with the STM32F4 Family of MCU's, a Linker Script is generated with a license that does not allow the code to be used with anything other than "System Workbench". ** (c)Copyright Ac6. ** You may use this ...

BCarl by Associate
  • 1154 Views
  • 1 replies
  • 0 kudos

Exclamation mark in STM32Cube

Hi everyoneI am new in ST ARM area in I am working on one design.Using STM32Cube tool I managed to locate all my resources, but I am not sure if it is OK and I need confirmation.I have some amber exclamation signs (no red), I suppose that my design ...

SFazl by Associate
  • 2935 Views
  • 3 replies
  • 0 kudos

CubeMX project for One-Pulse Mode example

Hi,Examples projects for STM32F4 are great by there is not the CubeMX projects associated.I am looking the CubeMX project of the TIM_OnePulse example for STM32F411RE-Nucleo.Is somebody has that ?ThanksLionel

Lionel1 by Associate II
  • 1239 Views
  • 2 replies
  • 0 kudos

STM32 USB Virtual com implementation

Hello,Using CubeMX, I have created USB CDC device for FS and started using the CDC.By modifying CDC_Receive_FS() I am able to receive all data sent form the PC over USB and put the data in my bufferAlso (while the USB cable is connected and PC termin...

CUBEMX EXTI17 bug

I have a project on CubeMX v5.0.1 - stm32 f103c8 that uses the RTC. I want an alarm interrupt on EXTI_17. In Cubemx under RTC I check Activatet he clock source, Select RTC output On Tamper Pin, and under NVIC, select RTC alarm interrupt through EXTI...

How to use i2c functions with stm32f401RE?

Hi, I'm using stm32f401RE and making a code with cubeMX.So I set i2c3 and I was going to get some numbers from LSM303DLHC whic is accelo/gyro sensor.Here's the codes what I set.​#define Slave_addr (0x1E<<1)#define X_high 0x03#define X_low 0x04uint8_t...

dlee.0 by Associate II
  • 1319 Views
  • 1 replies
  • 0 kudos