STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

stm32cubemx example code not able to receive

#include "main.h" #include "stm32f4xx_hal.h"   /* USER CODE BEGIN Includes */   /* USER CODE END Includes */   /* Private variables ---------------------------------------------------------*/ CAN_HandleTypeDef hcan1;   /* USER CODE BEGIN PV */ /* Pri...

kgedi by Associate II
  • 982 Views
  • 0 replies
  • 0 kudos

STM32CubeMX and B-L475E-IOT01A SPI2

I am using STM32CubeMX v5.0.1 on Windows10. I am trying to set up the B-L475E-IOT01A board's SPI2 port to communicate with a SPI based PMOD device. The user manual for the board shows SPI2 to be the port that connected to PMOD. STM32CubeMX will no...

ptracton by Associate II
  • 1151 Views
  • 1 replies
  • 0 kudos

Settings lost when changing MCU

Hi,I am in the stage of porting an existing STM32F4 design to STM32CubeMX and in the future upgrade to a pin compatible STM32F7. STM32CubeMX seems to be a great tool with lot of potential but I have an issue when changing to a "Full Compatible" MCU u...

SAnde.12 by Associate
  • 680 Views
  • 0 replies
  • 1 kudos

Help establishing USART Receive Interrupt

We are using the NUCLEO-F091RC and need help establishing a working demo of a USART-Rx interrupt. We have put much effort into this with no success, here is the process we are at:   Demo Attempt Process:Open CubeMX->Board Selector->NUCLEO-F091RCDefau...

Justin1 by Senior
  • 689 Views
  • 1 replies
  • 0 kudos

what are the necessary configurations needed for can protocol

i had intialized can1 and can2 of my stm board but after writtingthe whole code only transmission of messages is happening on both the boards but not the receiving.but when iused one board for transmission and one for reception its working properly.s...

AGaja by Associate II
  • 2156 Views
  • 4 replies
  • 0 kudos

I can't seem to get STM32CubeMX to start.

It gives a dialog that says some path is missing in the registry or the JRE is corrupt. I tried removing and reinstalling JRE, then reinstalled CubeMX. Nothing seems to help. There were some entries in the registry under JavaSoft. Seems like CubeMX n...

RBlac by Associate
  • 574 Views
  • 0 replies
  • 0 kudos