STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1626 Views
  • 0 replies
  • 2 kudos

New CubeMX (5.4.0) is extremly slow!

On my i7-4Core Notebook with SSDs and 32GByte RAM,newest Java Version:Starting Program: 5-7 MinutesOpen existing Project (F767zit, All 144 Pins used): 10 MinutesDeactivating TIM7: 1-2 MinuteChanging Pin Function: 1-2 MinuteGenerating Code is normal i...

KLamb.4 by Associate
  • 1797 Views
  • 3 replies
  • 2 kudos

Using STM32CubeMX I want to configure FATFS Middleware in SD Card Mode, but the checkbox for SD Card is grayed out although I have configure SDIO connectivity

I am using CubeMX Version 5.4.0.I tried MMC 4bit and SD 4bit for SDIO configuration but both did not enable SD card mode for FATFS. What are the exact conditions that need to be fulfilled to allow FATFS using SD card mode?

How to bring CMSIS DSP LIb into vanilla Cubemx project?

HiI am trying to correctly include the CMSIS DSP Library into Cubemx project. I went threw the forums and look at what ever documentation I could find.​IDE used STCUBEIDE​.​I​ have noticed that the F4 and F7 that has DFSDM support allow enables the C...

NHend.7 by Associate II
  • 1090 Views
  • 0 replies
  • 0 kudos

Resolved! STM32CUBEMX aspect is getting worse and worse

Can someone explain to me how I can do to be able to view all the settings? The cursor is on the edge and there are still too many settings to list that I can't see.Since they released version 5, CubeMX has become increasingly confusing and difficult...

0690X00000Aqem9QAB.png

CubeMX suggestion - keep user pin labels

While you are at the CubeMX improvements...Please preserve the user label, when the pin mode changes.Often times I need to fix wrongly assigned mode - analog to input or output or EXTI and so on.The Cube resets the user label when the mode changes. I...

Pavel A. by Super User
  • 1012 Views
  • 1 replies
  • 0 kudos