STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1626 Views
  • 0 replies
  • 2 kudos

STM32F413VG, I am not able to work SPI over DMA or Interrupt. I can do it in a polling way which is not an option for my case.

I have followed many of tutorials on the web.I have problems using SPI via DMA and IT. There is no data flow. But it works using polling.In addition to this, UART also is not functional over DMA.My CubeMX version is 5.4.0.I have watched tutorials bel...

Automatic way to bring related pins "close" together?

Sometimes related pins get automatically mapped in different physical locations on the chip. When possible given alternate pin map choices, I would like related pins near each other for PCB routing purposes. It takes a long time to search all the pin...

Keil Project file have generation problem.

Im currently using last verison of CUBEMX , when I creating project keil project file have been generation problem.I re-installed program,Changed path of CUBEMX as C/: as well as shorth pathway with english characters.Thanks A lot

Proteus by Associate II
  • 1806 Views
  • 4 replies
  • 0 kudos

How to get IP with Nucleo-H743ZI stm32CubeIDE, using lwip?

Hello,I have the Nucleo-H743zi board and I am trying to use lwip+rtos to create a socket client, but I can't get IP. I added FreeRTOS, but there are no specifications on the parameters used in order to get IP address. I tried to use the parameters th...

Angelos1 by Associate II
  • 3320 Views
  • 4 replies
  • 0 kudos

Resolved! UART transmit error character

Hello,i have problem for using STM32H743VI. start from the basic problem, that is transmit UART standard. i use latest firmware of STM32H7 version 1.5.0, latest update STM32CUBEIDE 1.1.0 and latest update STM32CUBEMX 5.3.here the code:int main(void){...

0690X00000ArRaqQAF.png 0690X00000ArRb0QAF.png 0690X00000ArRbAQAV.png 0690X00000ArRb5QAF.png
mal h by Associate II
  • 2868 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CubeMX not working to switch to another MCU

I am following the instructions in the 'UM1718 User manual", section 10.9, "Switching to another MCU".In STM32CubeMX I opened a new project and chose the F303RETx MCU option. Then I imported a working .ioc file into STM32CubeMX that was originally se...

CLee.0 by Associate III
  • 2043 Views
  • 3 replies
  • 0 kudos