User Activity

Hi all!Been a loooong time since I've been around forums, but I'm back!So a long time project I've wanted to do is coming back into my brain and I figure its time to start chipping away at it!I love RGB LEDs, especially the addressable variety, and I...
Hi All,I have downloaded the latest version of the fatfs library from http://elm-chan.org/fsw/ff/00index_e.htmlI have a project with the fatfs middleware running, the project was created via cubemx. So far I have had no issues with the librabry, howe...
Hi All,I am currently working on creating a file system on an stm32f207, using the nucleo board for the time being while I wait for my custom boards.The board will have an SD card as well as a USB. I have made a simple function for creating a folder ...
Hi all,I am having troubles mounting a USB using the "f_mount" function in the fatfs library. My usb does mount but only after many attempts, using a simple counter I have found it to be 81, every single time I run the code it is the same amount of a...
Hi all,I am currently learning how to interface with a USB using an stm32f2 as a host.I am using the fatfs library and it is working quite well.I have a question relating how removing a USB from the system. Similar to Windows for example, they have a...
Kudos from