STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1560 Views
  • 0 replies
  • 2 kudos

CubeMX LL build failure

I am using a custom board that uses the STM32F769NI chip. I am finding that any attempt to build using the LL drivers causes build failures. I suppose this is a bug, but not sure if or how to report.For the attached reference mx project, it fails w...

_EFrie by Senior
  • 2205 Views
  • 4 replies
  • 0 kudos

Installing STM32CubeMx on OpenSuse Tumbleweed

Installing STM32CubeMx on OpenSuse Tumbleweed using /st-stm32cubeide_1.1.0_4551_20191014_1140_amd64.rpm_bundle.sis missing libusbxsudo ./st-stm32cubeide_1.1.0_4551_20191014_1140_amd64.rpm_bundle.sh [sudo] Passwort für root: Creating directory st-st...

hj by Associate III
  • 1242 Views
  • 1 replies
  • 0 kudos

STM32H747 Hardware Semaphore Interrupt

EDIT: Nevermind this thread can be deleted, apologies. I didn't enable the HSEM2 Global interrupts under NVIC1/2 in CubeMX.Hi,I'm having issues getting the hardware semaphore interrupts to function correctly, or I'm misunderstanding their usage. I'm ...

savvn001 by Associate II
  • 1746 Views
  • 1 replies
  • 0 kudos

Building file systems/projects with STM32CubeMX

Hello, I bought the STEVAL-IDP003V1D evaluation board and I want to create a "custom" IO-Link slave device that, I can hook up to an existing IO-Link Master. Then write commands from the master and receive a response from my slave. I found the IO-Lin...

Soepoe by Associate II
  • 812 Views
  • 1 replies
  • 0 kudos