STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

FreeRTOS 10.1.1 Upgrade in STM32CubeMX

Hi all,When I click on the little "i" (info) icon in the FreeRTOS configuration screen in CubeMX, I get the following message: Current version shows as 10.0.1 and under Diagnostic, it says "New version available for L4". Indeed, I checked on FreeRTOS...

0690X000006CStgQAG.png

Clock configuration for USB on STM32F746ZE

Hi all,I'm using an STM32F746ZE in my application that uses USB OTG HS with internal FS Phy in Host only configuration.Originally, I have setup the clock in the following manner:in order to have 48MHz clock for USB. With this configuration, any devic...

0690X00000DC0BFQA1.png 0690X00000DC0CcQAL.png
EBris.1 by Associate
  • 1430 Views
  • 0 replies
  • 0 kudos

I2C SCL operating frequency is very low. I configured the I2C2 Interface of my STM32F103 to have a clock frequency of 100 KHz (standard Mode) but it turns out to only be around 4 kHz. Can you point me in the right direction as why this could happen?

I am using the STM32F103C8T6 Microcontroller to read a sensor via I2C. I am using the stm32Cubemx to generate the initialisation code and Visual Studio and VisualGDB for debugging. My STM32CubeMX setup reads as follows:and my clock configuration:But ...

0690X00000DBuO8QAL.png 0690X00000DBuOwQAL.png 0690X00000DBuPzQAL.png
TKöhl.1 by Associate II
  • 3938 Views
  • 4 replies
  • 0 kudos

CubeMX - FATFS on SD-card for V2 Interface.

In CubeMXthere is not possible to select SD-Card support in FATFS if CMSIS V2 interface is selected for FreeRTOS.It worksonly for CMSIS V1.Are there any plans to support FATFS on SD-card for V2 Interface?

BUG: The __HAL_LOCK(x) macro needs a lock.

I can only imagine that __HAL_LOCK(x) is designed to make access to the HAL drivers thread safe. However, since the lock itself is not thread safe, the driver it's trying to protect is not thread safe either.I've spent a day trying to work out how t...

DOsbo by Senior
  • 2503 Views
  • 1 replies
  • 0 kudos