User Activity

Hello,I was wondering how hard is to convert the simple OpenAMP_TTY_echo (I have it installing the STM32Cube_FW_MP1_V1.6.0 package from STMicroelectronics' web site) to a Makefile driven project.I need it so, because the firmware auto building of my ...
Hello everyoneI am struggling with my custom board to be used as HOST or DEVICE.In my board I have both connectors USB HOST A, and miniUSB Device connector in parallel.When using an application as USB HOST for an USB Keyboard, everything is working f...
I would like to bring up the openocd and gdb debugger on a custom board with STM32MP157D processor with 1 GB (2x512MB 16 bit DDR3 chips) x 32 bit. The modified device-tree and SPL gives me the following issue:U-Boot SPL 2022.01-rc3 (Sep 07 2022 - 16:...
Hello,I am trying to bring up a custom board based on the STM32MP157D MPU via SDCard.I am using u-boot 2022-01-rc3 as bootloader and the boot is using SPL (I have an SDCard with a GPT Partition table with fsbl1, fsbl2 and ssbl named partitions).This ...
Hello,I would like to know why if you are building a project with code-generated makefile for the MCU STM32F407IGTx (QFP176 pins) the linker file STM32F407ICTx_FLASH.ld tells the compiler the RAM origin at 0x20000000 has a length of 128K instead of 1...
Kudos from