STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

Resolved! Setting VREF voltage in CubeMX not working for STM32G4

I'd like to report 2 bugs/errors in CubeMx and the documentation in the stm32g4xx LL driver file:Setting the "Internal Voltage reference scale" in the "SYS" menu of CubeMX to SCALE2 (2.9V), won't take effect and the selected value always falls back t...

MScho.1 by Associate III
  • 3700 Views
  • 6 replies
  • 0 kudos

STM32CubeMX: generate buggy SystemClock_Config() ?

Using STM32Cube MX 5.5.0 and STM32Cube FW_H7 V1.6.0 I observed two curious things1) When I use LL drivers to generate a project, the function SystemClock_Config() contains:/* Intermediate AHB prescaler 2 when target frequency clock is higher than 80...

Ethernet failed over RTOS on Board NucleoF767ZI

Hi All, I have a problem on Ethernet connection while using RTOS, I tried to figure it out but no positive result. Everything is fine (Ethernet is working) until I use RTOS. I tried to find the solution in CubeMX example package, and this article htt...

I am working with STM32F407VGt6-DISC1, I am facing a problem in getting LSE clock frequency out of MCO1 pin, and also other external source of clock whereas the same process for internal clock measurement through i worked fined.

Here i attached my main.c file.andWhen I run my debugger , i see that my program is stucked in error handler//////////if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK){_Error_Handler(__FILE__, __LINE__);}//////////And for measuring internal clock ...

VChou.1 by Associate
  • 1955 Views
  • 1 replies
  • 0 kudos