User Activity

Hi,I am unable to update embedded software packages.To update I select "Manage embedded software packages" menu item. Packages manager window opens. I see "Check Firmware & Software. Download File updaters.zip" but progress bar stays at 0 bytes. Afte...
After updating to STM32CubeIDE 1.2.1 I cannot open anymore .ioc file in STM32CubeMX device configuration tool. When I double click on existing .ioc in the project text editor opens instead of STM32CubeMX.
Hi,recently I installed STM32CubeMX. When I click 'Check for update' menu item 'STM32CubeF1 Firmware Package V1.7.0 / 09-October-2018' is shown. But when I press 'Install Now' the following error happens:In the log I see:2018-11-20 23:56:39,197 [ER...