STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1628 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX Pin Re-assignment on STM32U5A9 - Questions

Hello Forum,I've noticed a feature/bug/behaviour in CubeMX 6.15.0 that I'm unsure about so could do with some advice.  I've been configuring an STM32U5A9ZJT 144 pin MCU for a project I'm working on.  This has been an evolutionary process.  To make th...

DenzilDexter_3-1761228001020.png DenzilDexter_4-1761228032426.png DenzilDexter_5-1761228137055.png DenzilDexter_6-1761228230738.png

Resolved! Losing Ethernet ETH_CLK settings

In my project for an STM32H7S3, I'm using the Ethernet module, and it works fine.However, I don't need the ETH_CLK pin. In RCC settings, there's an option which suggests I can turn it off; however, clicking the tickbox has no effect. (Note also that ...

SteveMelnikoff_0-1752584425356.png

Will the FTP addon for AZRTOS work for an F7 chip?

I'm looking to utilize an FTP server with the STM32F7NI-Discovery board. Specifically I'm looking at taking Nx_Webserver demo for that board (which works great) and adding the ftp module to it that NetxDuo provides. However, I'm seeing that the F7 ch...

ijohnson_0-1760718396710.png ijohnson_1-1760718438588.png
ijohnson by Associate
  • 482 Views
  • 1 replies
  • 0 kudos

assert_param(expr) defined in two files?

I have a project for STM32F777 generated by STM32CubeMX 6.15.0.The macro definition of #define assert_param(expr) exists in 2 include files - stm32f7xx_hal_conf.hand stm32_assert.hBoth files are included on different levels of the project. Is there a...

Ceco by Associate II
  • 447 Views
  • 2 replies
  • 0 kudos