I'm new to STM32CubeMX and have difficulties finding out how to map all OCTOSPIM_P2 signals to Port G. I can manually map some signals to Port G (CS, IO[7:4], DQS), but can't figure out how to map the rest. Any help most welcome!
We are designing a board for internal product development and testing (not for sale) based on NUCLEO-U575ZI-Q (the Altium source). We aim to manufacture a handful of boards for internal use during development. We will re-use parts of the existing des...
Hi,as the question indicates, I wonder what the max (rated?) speed on SPI is if the Nucleo board is connected to a carrier board (with very short leads with proper SI) to a SPI master/slave device. I searched for information on the ST Zio connector c...
Thanks for the feedback @KDJEM.1It appears that it is not possible when reading Table 27. However, that means that the text in para 3.28 is a bit misleading:Since we consequently are forced to run the entire CPU on 1V8, is it correct that we can run ...