STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1588 Views
  • 0 replies
  • 2 kudos

Resolved! Enable MPU on NUCLEO-G474RE project

The data sheet for the G474RE says it has a Memory Protection Unit. The article on how to enable/configure it in STM32CubeMX shows a CORTEX_M# node under "System Core". I don't see that node. Thank you.

Eric_S0 by Associate
  • 130 Views
  • 1 replies
  • 1 kudos

Resolved! FDCAN configuration in STM32N6 Nucleo

Hi! I'm working on setting up FDCAN communication using the STM32N6570X0-Q Nucleo Board. However, when I try to modify the bit timing parameters—such as the Nominal Prescaler, Nominal Time Seg1, or Seg2—the baud rate doesn't seem to change regardless...

guillerminaborrazas_0-1754334467731.png

Resolved! Possible Cube MX wrong specs & package for STM32C051K8 ?

Hi,when selecting the STM32C051K8 in Cube MX it seems that CubeMX has wrong configs/specs about it?As you can see from the screenshot below it shows it is a LQFP package but - unless I missed something - it is supposed to be a UFQFPN32 package.The ma...

Ricko_1-1777503759957.png
Ricko by Senior III
  • 199 Views
  • 2 replies
  • 2 kudos