2025-07-22 8:43 PM
void MX_WWDG_Init(void)
{
/* USER CODE BEGIN WWDG_Init 0 */
/* USER CODE END WWDG_Init 0 */
/* Peripheral clock enable */
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_WWDG);
/* USER CODE BEGIN WWDG_Init 1 */
/* USER CODE END WWDG_Init 1 */
LL_WWDG_SetCounter(WWDG, 64);
LL_WWDG_Enable(WWDG);
LL_WWDG_SetPrescaler(WWDG, LL_WWDG_PRESCALER_1);
LL_WWDG_SetWindow(WWDG, 64);
/* USER CODE BEGIN WWDG_Init 2 */
/* USER CODE END WWDG_Init 2 */
}
void MX_IWDG_Init(void)
{
/* USER CODE BEGIN IWDG_Init 0 */
/* USER CODE END IWDG_Init 0 */
/* USER CODE BEGIN IWDG_Init 1 */
/* USER CODE END IWDG_Init 1 */
LL_IWDG_Enable(IWDG);
LL_IWDG_EnableWriteAccess(IWDG);
LL_IWDG_SetPrescaler(IWDG, LL_IWDG_PRESCALER_4);
LL_IWDG_SetReloadCounter(IWDG, 4095);
while (LL_IWDG_IsReady(IWDG) != 1)
{
}
LL_IWDG_ReloadCounter(IWDG);
/* USER CODE BEGIN IWDG_Init 2 */
/* USER CODE END IWDG_Init 2 */
}
int main(void)
{
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SYSCFG);
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
NVIC_SetPriority(SysTick_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 15, 0));
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_USART1_UART_Init();
char data[128];
static int startup_count = 0;
sprintf(data, "Startup count: %d\n", startup_count++);
UART_SendData((const uint8_t*)data, strlen(data));
MX_WWDG_Init();
MX_IWDG_Init();
while (1)
{
WWDG_Feed(); // Feed WWDG first
IWDG_Feed();
LL_mDelay(10);
sprintf(data, "Loop running, count: %d\n", startup_count++);
UART_SendData((const uint8_t*)data, strlen(data));
}
}
Cutecom shows "Startup count: 0" forever and WWDG_Feed() and IWDG_Feed() not called since system reset before entering while() loop.
2025-07-23 5:22 AM
WWDG must be refreshed within a particular window. You're refreshing too early which leads to the reset.
The code you attached doesn't match the code in your post.
void MX_WWDG_Init(void)
{
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_WWDG);
LL_WWDG_SetPrescaler(WWDG, LL_WWDG_PRESCALER_8); // Divide PCLK1 by 8
LL_WWDG_SetCounter(WWDG, 127); // Start at max counter value
LL_WWDG_SetWindow(WWDG, 80); // Allow refresh when counter is >= 80
LL_WWDG_Enable(WWDG);
}Based on these settings, you must refresh the WWDG when the counter is lower than 80 and above 64 (code comments are wrong).
2025-07-23 5:35 AM
Thanks for your reply. Does ST provide API to check if WWDG can be refresh or how to implement it by myself?