2025-07-23 11:19 AM
I just updated CubeMX to 6.15.0 and I can't start a new project anymore.
The spinning wheel keeps sinning forever after going File/New Project or clicking on any on the shortcuts on the right side of the screen under "I need to:" section.
I tried to refresh data, use auto-refresh under connection and updates, etc. Nothing works.
I'm on Windows 11 Home, Version 24H2.
Older projects still work after conversion, I can still open older .ioc projects, but the dialog is asking me to migrate the project and I don't want to do that in case I need to downgrade the CubeMX application.
Is there a way to downgrade to a pervious version?
Thank you!
2025-07-23 7:04 PM
I got it to work after uninstalling and re-installing everything.