User Activity

Hello, I have a question about LWIP functionality.I'd like to know if it's possible to redirect a tcp request received on the pppos interface, to a device that is connected onto the ethernet interface and listening on the desired port.Thanks in advan...
Hello everyone,I'm using Netconn snmp over freertos on my project and I found an issue when using 2 netif interfaces. The problem is that when I receive udp messages, the response is always routed to the default netif despite having the LWIP_HOOK_IP4...
Hello everyone,Today I'm writing to you because I'm trying to implement a PPPoS connection over the USB CDC Host of a STM32H745. The modem I'm trying to connect to is a SIM7500 of SimCom.I managed to establish the connection between the modem and the...
Hi, I am trying to use a Nucleo-H745ZIQ to implement the USB CDC HOST functionality over the USB OTG FS port. I succeeded to do it and make it work if the device connected to my board is another STM32 board which is configured as an usb device, and t...
Kudos from
Kudos given to