STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1572 Views
  • 0 replies
  • 2 kudos

STM32CubeMX 5.6.0 Hangs at "Generating user source code..."

I have recently upgraded to STM32CubeMX 5.6.0 and created a new project based around the STM32H753ZITx family.I can usually get one "Generate Code" operation when the PC has freshly booted up, but if I try and "Generate Code" subsequent times it just...

Matt.1 by Associate II
  • 3034 Views
  • 4 replies
  • 0 kudos

H7 NUCLEO CubeMX-based application running. About 85% done. SW4STM32 dev continues. Custom board with H7 MCU now built. Do I need a new MCU-only (not NUCLEO) -based Cube project or will code built from original NUCLEO-based Cube project flash and run?

More detailed description and questions:1) MacBook Pro, CubeMX 5.4.0, SystemWorkbench 4.6.3.2) Program for NUCLEO-H743ZI board, CubeMX generated and built. Still some development work to do ..3) However, now have the prototype's custom board which in...

APagl by Associate III
  • 1032 Views
  • 2 replies
  • 0 kudos

STM32F407 HAL_SPI_DMA usage for halfword to halfword transfer

HiI am trying to construct an SPI based device driver for an ADC which has 16 bit Frame size .The examples provided for SPI DMA showcases the use of uint_8 * buffers//HAL_SPI_TransmitReceive_DMA(&SpiHandle, (uint8_t*)aTxBuffer, (uint8_t *)aRxBuffer,...

RK.1 by Associate II
  • 2226 Views
  • 3 replies
  • 0 kudos

AD9833 Module Control

Hello,I want to control the ad9833 module with the stm32f4 development board. I have a library but I couldn't get SPI communication. I cannot get any wave output from the module. I cannot adjust frequency. where can the problem be? I need to create t...

BTaşk.1 by Associate II
  • 4876 Views
  • 5 replies
  • 0 kudos