STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1592 Views
  • 0 replies
  • 2 kudos

Resolved! Override default I2C GPIO settings in CubeMX?

Hi,I'd like to override the GPIO settings for the I2C GPIOs. For example, I want to disable pullups and change the drive strength. In the CubeMX GUI there's not option to do this. So far I've just modified the code that gets generated but annoyingly ...

DBurr by Senior
  • 1703 Views
  • 2 replies
  • 0 kudos

Code Generator not generating Code on GPIOs for SDIO?

Dear all,i have a F412 and SDIO enabled (1Bit). Also, set the corresponding GPIOs to pullup in the GPIO settings. However, I do not see generated code to initialize these Pins at all (they are not showing up). Tried removing them and adding again - n...

SSchu.4 by Associate II
  • 1085 Views
  • 4 replies
  • 0 kudos

What families have oversampling on the ADC(s)?

I thought I ran into a bug when CubeMX could not configure oversampling for an F767 after I had used it on the less powerful L4. Read the reference manual and understand it is not there. Could not find which non-L families DO have oversampling. Hence...

Fanuc30 by Associate III
  • 1474 Views
  • 2 replies
  • 0 kudos