STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

STM32F427 I2C no SCL output and *Very* slow SDA output

Hi everyone,I've been working on a custom PCB with an STM32F427 and a TI audio amp (TAS5825M) that need to communicate using I2C. This is my first time using the STM32 line. I set up the project with STM32CubeMX with the appropriate settings for 100 ...

0693W000001qNX1QAM.png 0693W000001qNY9QAM.png
PGrin.1 by Associate
  • 2220 Views
  • 3 replies
  • 0 kudos

Resolved! Hi I am using the STM3241G-EVAL board with an ethernet connection. I want to create an http based application using TCP/IP. I used STM32 CUBE MX to generate code with settings ETH(MII mode) ,LWIP enabled with DHCP.

My code is not passing the netif_is_link_up() function and it always goes to netif_set_down(). I also have this doubt when I connect network cable to Ethernet port of board, it does not glow any green or yellow light on this port. But my network cabl...

MHans.2 by Associate II
  • 1546 Views
  • 2 replies
  • 0 kudos

Resolved! Hello All I am using STM32CUBE MX, version 5.6 for controller STM32G474RE so I wich to connect the OPAMP2 and OPAMP3 to the ADC internally. But I can not to find this adjustment in the CUBE software. Can some body answer me, how to do it with CUBE?

So I can not enable internal connection by CUBE and VOUT occupies some pin on the PInOut View which I intend to use for other purpose, so I can not to use all advantages of CUBE . So The Configuration page of OPAMP look like attached pictuire

0693W000001qWheQAE.png
AShev.1 by Associate II
  • 1584 Views
  • 3 replies
  • 0 kudos

Cube MX does not create a project

it does not create a project. I used this ioc file on a working computer,There it earned. How to fix my cube mx? or reinstall Keil 5? I need help. I add Keil project

AArt.1 by Associate II
  • 2957 Views
  • 3 replies
  • 0 kudos

makefile:43 error pls help

Hi!I am trying to create a very first Hello World project like that:/** ****************************************************************************** * @file      : main.c * @author     : Auto-generated by STM32CubeIDE * @brief     : Main program bo...

M.umit by Associate II
  • 2785 Views
  • 4 replies
  • 0 kudos