cancel
Showing results for 
Search instead for 
Did you mean: 

How to get UART DMA interrupt to work?

AGarp.1
Associate II

I have implemented the following code based on some examples on internet. It is supposed to trigger the DMA transfer complete callback put it does not. 99% of the code is generated using CubeMX IDE.

 The modified part of the code:

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
	HAL_GPIO_TogglePin(GPIOA, LD2_Pin);
}
 
/* USER CODE END 0 */
 
/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */
 
  /* USER CODE END 1 */
  
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_USART2_UART_Init();
  MX_DMA_Init();
  /* USER CODE BEGIN 2 */
  uint8_t pData[16];
  HAL_UART_Receive_DMA(&huart2, pData, 16);
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}

Autogenerated DMA init:

static void MX_DMA_Init(void) 
{
 
  /* DMA controller clock enable */
  __HAL_RCC_DMA1_CLK_ENABLE();
 
  /* DMA interrupt init */
  /* DMA1_Channel6_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA1_Channel6_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(DMA1_Channel6_IRQn);
 
}

What Im I doing wrong? The code I generate is basically the same as in examples across internet. I have a nuceo-L476RG board. Below is the CubeMX project attached:

Best,

Anders

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
T J
Lead

       (++) DMA Configuration if you need to use DMA process (HAL_UART_Transmit_DMA() and HAL_UART_Receive_DMA() APIs):

           (+++) Declare a DMA handle structure for the Tx/Rx channel.

           (+++) Enable the DMAx interface clock.

           (+++) Configure the declared DMA handle structure with the required Tx/Rx parameters.

           (+++) Configure the DMA Tx/Rx channel.

           (+++) Associate the initialized DMA handle to the UART DMA Tx/Rx handle.

           (+++) Configure the priority and enable the NVIC for the transfer complete interrupt on the DMA Tx/Rx channel.

AGarp.1
Associate II

Thanks for the tip! Indeed it was the CubeMX placing the initialisation in the wrong order.