2019-10-09 3:59 PM
Specifically, for a STM32F723, with the HS USB PHY enabled, it's giving me an error in
HAL_StatusTypeDef USB_WritePacket(USB_OTG_GlobalTypeDef *USBx, uint8_t *src, uint8_t ch_ep_num, uint16_t len, uint8_t dma)
{
uint32_t USBx_BASE = (uint32_t)USBx;
uint32_t *pSrc = (uint32_t *)src;
uint32_t count32b, i;
if (dma == 0U)
{
count32b = ((uint32_t)len + 3U) / 4U;
for (i = 0U; i < count32b; i++)
{
USBx_DFIFO((uint32_t)ch_ep_num) = *((__packed uint32_t *)pSrc);
pSrc++;
}
}
return HAL_OK;
}... where it's the __packed that's causing the problem. The same thing is true for the USB_ReadPacket immediately below the above in stm32f7xx_ll_usb.c
I'm not sure what the effect of removing the __packed will be (presumably it's there for a reason!) but after freshly generating the project, a build produces:
../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_usb.c: In function 'USB_WritePacket':
../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_usb.c:958:53: error: expected ')' before 'uint32_t'
USBx_DFIFO((uint32_t)ch_ep_num) = *((__packed uint32_t *)pSrc);
^~~~~~~~
../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_usb.c:958:64: error: expected ')' before 'pSrc'
USBx_DFIFO((uint32_t)ch_ep_num) = *((__packed uint32_t *)pSrc);
^~~~
../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_usb.c: In function 'USB_ReadPacket':
../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_usb.c:987:16: error: expected ')' before 'uint32_t'
*(__packed uint32_t *)pDest = USBx_DFIFO(0U);
^~~~~~~~
../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_usb.c:987:5: warning: statement with no effect [-Wunused-value]
*(__packed uint32_t *)pDest = USBx_DFIFO(0U);
^~~~~~~~~~~~~~~~~~~
../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_usb.c:987:27: error: expected ';' before 'pDest'
*(__packed uint32_t *)pDest = USBx_DFIFO(0U);
^~~~~
../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_usb.c:980:12: warning: unused variable 'USBx_BASE' [-Wunused-variable]
uint32_t USBx_BASE = (uint32_t)USBx;
^~~~~~~~~
make: *** [Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_usb.o] Error 1Removing the __packed attribute from both calls makes it compile cleanly.
2019-10-15 6:18 PM
This time around I'm trying to generate a build for ST's own STM32F723E-DISCO board, selected defaults, chose sw4stm32. I thought I might have better luck with an official board from ST.
Nope. Same problem.
So after much searching, I found the reason for this - it seems that STCube defines __packed surrounded with quotes, which is simply wrong. It can be fixed by selecting the project, going to Project -> Properties -> C/C++ General -> Symbols : Remove quotes around __packed and __weak
At which point, the build will fail because it can't find os_tick.h. Great. Ok "find" to the rescue, get the path and configure it in Project -> Properties -> C/C++ General -> Includes : Add Drivers/CMSIS/RTOS2/Include
At which point it fails saying it can't find RTE_Components.h. Ok, another find. Ah - there's lots of them...
find . -name RTE_Components.h ./Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/cifar10/RTE/_ARMCM0/RTE_Components.h
./Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/cifar10/RTE/_ARMCM3/RTE_Components.h
./Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/cifar10/RTE/_ARMCM4_FP/RTE_Components.h
./Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/cifar10/RTE/_ARMCM7_SP/RTE_Components.h
./Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/gru/RTE/_ARMCM0/RTE_Components.h
./Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/gru/RTE/_ARMCM3/RTE_Components.h
./Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/gru/RTE/_ARMCM4_FP/RTE_Components.h
./Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/gru/RTE/_ARMCM7_SP/RTE_Components.h
./Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/_ARMCM0/RTE_Components.h
./Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/_ARMCM3/RTE_Components.h
./Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/_ARMCM4_FP/RTE_Components.h
./Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/_ARMCM7_SP/So let's assume it's the one in ./Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/_ARMCM7_SP - and add that path to Project -> Properties -> C/C++ General -> Includes as well...
And then it fails with "Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/_ARMCM7_SP/RTE_Components.h:17:29: fatal error: ARMCM7_SP.h: No such file or directory"
Ok, well it's got me there, doing a 'find . -name ARMCM7_SP.h' returns nothing, nada, zilch, zero point...
At this point I have to give up. This is the latest version of STMCube and it's just generating very broken code. Sigh.
2019-12-24 4:36 AM
Simply remove in your Project Properties > C/C++ Build > Settings > MCU GCC Compiler > Preprocessor > Defined Symbols the line
__packed__="__attribute__((__packed__))"
I also added the line USE_USB_FS.
This solved my problem to use USB sticks.
2019-12-24 6:15 PM
Could anybody explain what exactly does __attribute__((packed)) for pointers?
Is it just a reminder for a programmer that the pointer or structure members are not aligned?
Or the compiler will actually generate code to access unaligned data by bytes and reassemble?
-- pa