Currently, i working on the nucleo-L552zeq and i run the SBSFU exemple propose by the cubeL5. i use the script regression.sh and the script the SBSFU_UPDATE.sh to initialize the board and download the firmware. this example can work normally on the b...
Hi All,i'am beginner of using libary HAL, i use CubeMX to generate code. At first, I use usart1 to send message and i work, and then i try to use usart2 but i cant can't send any message.these two code is almost the same.