STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1556 Views
  • 0 replies
  • 2 kudos

Resolved! Can't load X-CUBE-53L0A1

I'm using STM32CubeMx 6.0.0 to develop for our STM32L4 board with a VL53L0X sensor on I2C. The X-CUBE-53L0A1 package is not listed, and attempting to load the zip file fails. Is this package supposed to be loadable? Or will I have to figure out how t...

lee23 by Associate II
  • 1801 Views
  • 1 replies
  • 0 kudos

stm32CubeMX 6.0.1 package install problem

Hi, I just installed the new CubeMX 6.01 version. When I download a software package via the package manager the zip is downloaded and unzipped but then the following message shows up: "Error downloading the following files:stm32_cube_fw_f4_v1250.zi...

DBrow by Associate II
  • 1189 Views
  • 1 replies
  • 0 kudos

Hi, I'm testing a CubeMX project for a stm32L010 proprietary board using HSI and LSI clock sources (default) on a nucleo-64 EVB; in both cases I have a problem of code immediately when running SystemClock_config() in main.c,

I don't understand what's wrong as only auto generated code is involved;  execution enters a dead lock waiting for a tick by HAL_GetTick() but no tick interrupt are invoked.

STM32CubeMX-5.2.1 installation path

STM32CubeMX-5.2.1 - why I can't install it in d:\STM32\STM32CubeMX path?I use d:\STM\ for \STM32 ST-LINK Utility\ , \STMStudio\ and other STM application. Why not CubeMX?Setup returns error: Invalid directory path. Please enter a directory path meets...

VPrib by Associate
  • 3625 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H753 lwip problem, STM32CubeMX v6, and STM32CUBE FW_H7 V1.8.0

Hello, I am trying to reproduce a Lwip project that was done on STM32CubeMX V5, and STM32CUBE FW_H7 V1.7.0. The project is very simple and consists of ethernet and lwip (httpd). The project works well on FW_H7 V1.7.0, but it does not compile on FW_H7...

VYoun by Associate III
  • 4926 Views
  • 5 replies
  • 1 kudos

arm_math.h with STMCUBEMX

I would like to use the DSP. Unfortunately it already fails because of the #include "arm_math.h".The file is not available in the project.Is there a suitable tutorial somewhere, everything I found so far does not work.I use a STM32F7 and STM32CubeIDE...

DMeix.1 by Associate II
  • 1672 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeMX Toolchains greyed out

I am using STM32CubeMX v6.0.1. I am designing for the chip STM32L552RET6. The problem is I want to output as a GPDSC file and the option is greyed out. If I select a different chip, I can select that toolchain no problem. How do I force the applicati...

RMcNa.1 by Associate
  • 2208 Views
  • 1 replies
  • 0 kudos

bug report for STM32CUBEMX 6.0

using stm32cubemx 6.0 to make a project for STM32F103RC TIM init.the configuration as follow pictures.the code be generated as a wrong as follow.stm32cubemx version 6.0STM32Cube_FW_F1_V1.8.0

0693W000003BZ7pQAG.png 0693W000003BZ7uQAG.png
Bruno Hu by Associate II
  • 2910 Views
  • 3 replies
  • 0 kudos