User Activity

Hi, I am trying to get a robust isochronous transfer of audio from my STM32F072CB using the audio device class. My code is based on the code generated by STM32CubeMX for a speaker but I have changed the descriptor in order to make it an audio input. ...
Hi,I use STM32CubeMX and SW4STM32 on my Macs. When I generate a project using CubeMx on my Mac running MacOSX 10.14 it loads fine into SW4STM32 and builds into a valid .bin. However, project files generated on my Mac running OSX10.15 does not compile...
The datasheet shows an n-channel mosfet between the IN_HV and L_HV pins of the SPV1050, but it seems to make more sense if this was a p-channel mosfet. For one thing, I don't think it is guaranteed that the chip will have a high enough voltage source...