STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

Resolved! STM32H7 + Keil + CubeMX?

Getting started with STM32H7, faced a problem. Ive worked for a long time with STM32F4 in Keil uVision (version 5.24.2.0), used a "classic" option, configuration via RTE_Device.h. Worked perfect.Now I dont have such option with STM32H7, only CubeMX, ...

Resolved! Can stm32f103 use C++?

Hi All,​Can stm32f103 use C++? for programing not c.​I'm using stm32f103 / truestudio / cubemx.​I want to use some c++ ​grammer for programing.If there's way to use c++How i can use c++ in stm32f103?regard.​​

Glee.11 by Associate II
  • 3151 Views
  • 4 replies
  • 0 kudos

Resolved! How to use just the HAL libraries in the STM32CubeIDE project without using CubeMX features and MX functions.

I want to a project from the scratch using the STM32CubeIDE for a STM32 Nucleo board. But I don't want to use the CubeMX feature of the IDE. I just to use the HAL libraries like we can do Ac6 workbench software. In Ac6 software, we have an option to ...

Resolved! [Fixed] Cant get ADC to work

Trying to read out a resistive touchscreen right now. To keep everything as simple as possible for testing I created an empty project in CubeMX just for testing this and set up all the pins in a static fashion (No reconfiguration at runtime)Measuring...

KK.2 by Associate III
  • 1555 Views
  • 2 replies
  • 0 kudos

Resolved! ST web site in Windows 10

In Windows 10 I visited www.st.com and accept the cookies and then all screen is changed to black and is not able to operate.I asked this question in Mac OS.

AXu.11 by Associate III
  • 2227 Views
  • 2 replies
  • 0 kudos

Resolved! Installation issue

When I install the STM32CubeMX in Windows 10 it prompts requiring Java 1.8.0_45(64-bit), in fact there is Java 1.8.0_261_b12 in my computer and my computer is 64_bit but it can't recognize.

AXu.11 by Associate III
  • 9910 Views
  • 9 replies
  • 0 kudos

CubeMX STM32H743 I2S Half Duplex Master

We have an issue with CubeMx and the I2S port. We set the port up as Half Duplex Master (so that the master clock goes out) and then in Configuration set the type to Master Receive. All good except that the two pins shows are CK and SDO. I am not sur...

FDixo by Associate III
  • 4080 Views
  • 7 replies
  • 3 kudos