STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

STM32CubeMX adds incorrect value to XTAL

Hello,I have been observing this issue with previous as well as latest STM32CubeMX versions, wherein the generated MDK-ARM (minimum version 5.27) project file (UVPROJX) has incorrect value set to Options for Target -> Target -> Xtal (MHz).In the IOC ...

Does STM32F723VC has a built in USB HS Phy?

USB HS PHY is quite confusing and i am not able to find out if i can use STM32F723VC (LQFP100) staight from the chip as a USB HS Device. Documentation says: "an USB OTG full-speed and a USB OTG high-speed with full-speed capability (with the ULPI onl...

nico by Associate II
  • 2372 Views
  • 4 replies
  • 0 kudos

Resolved! STM32 & CubeMX LWIP change IP

Hi, I use LWIP to establish a connection, We want to change the IP address, how can I update IP? tcpip_init( NULL, NULL );   /* IP addresses initialization without DHCP (IPv4) */ IP4_ADDR(&ipaddr, IP_ADDRESS[0], IP_ADDRESS[1], IP_ADDRESS[2], IP_A...

YiKai by Associate II
  • 2101 Views
  • 2 replies
  • 0 kudos

Resolved! After Stm32CubeIDE refresh I cannot save my IoC

Today I started my Stm32CubeIDE and I tried to create a new project. It refreshed itself, and after that I couldn't save ioc, and I couldn't switch to another .h or .c files. I had to kick out this application by task manager. I use Debian Linux & Ja...

ZZida.1 by Associate II
  • 1786 Views
  • 2 replies
  • 0 kudos

Interesting http iap in STM32CubeMX

STM32F4x7 in-application programming (IAP) over Ethernet based on LwIP TCP/IP stack (AN3968), it is possible to realize this with stm32cubemx. Maybe there are manuals like this done through STM32CubeMX?

MJere.1 by Associate
  • 1236 Views
  • 2 replies
  • 0 kudos