STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

I can't receive from uart3 and up on STM32F730R8

I want to use circular DMA to receive data of unknown length on 4 uarts of STM32F730R8, but I receive data just on first two of them. Transmission works and I use HAL library. Code is generated by MX configuration tool and all uarts are configured id...

AKapl by Associate
  • 1086 Views
  • 1 replies
  • 0 kudos

STM32 HAL FDCAN

Hello,Is it possibile to add four or more filters ? thanks in advance

FBern.2 by Associate II
  • 2753 Views
  • 5 replies
  • 0 kudos

Resolved! How to fix STM32CubeMX ver 6.0.1 on Linux Mint from throwing an exception when trying to create a new project?

I have started from the command line so I can see errors. It starts up ok but when I try to create a new project using "ACCESS TO MCU SELECTOR" it throws the error:Exception in thread "AWT-EventQueue-0" java.lang.NoSuchMethodError: com.st.microxplor...

Using CMSIS Packs with STM32CubeMX and IAR Embedded Workbench

I'm trying to use the CMSIS-Driver Interface to access Microcontroller Peripherals.As a starting point, i tried setting up an application with a simple goal: Transmit a byte using the USART Peripheral via CMSIS-Driver interface, which i can then use ...

MSchm.3 by Associate
  • 2901 Views
  • 0 replies
  • 0 kudos