STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1558 Views
  • 0 replies
  • 2 kudos

Resolved! I am having an issue with the latest version of Cube MX when generating the code. Would appreciate if anyone can help. I suspected it was where I was storing it I tried dropbox/onedrive/documents and even downloads and still getting the same issue.

Please see the images attached:Project Manager.Error Message after project generation.STM32 Cube MX logfile with Error Message.CUBE MX Version: STM32Cube MCU Package for STM32F4 Series 1.25.2Keil version: 5.27Thanks for your time.Best Regards,Luke

LMyle.1 by Associate III
  • 4812 Views
  • 6 replies
  • 0 kudos

STM32CubeMX couldn't be found error on Keil

Hello,I am trying to create a simple project on Keil and add some components via "Run Time Environment". I select necessary components then it tries to run STM32CubeMX which is also checked under "Device" tab. Anyhow, I get an instant error says that...

0690X000009Yp6yQAC.png
BDans by Associate
  • 4404 Views
  • 1 replies
  • 1 kudos

Resolved! Bug in RTC CubeMX code generate

static void MX_RTC_Init(void)   {       /* USER CODE BEGIN RTC_Init 0 */       /* USER CODE END RTC_Init 0 */       LL_RTC_InitTypeDef RTC_InitStruct = {0};   LL_RTC_TimeTypeDef RTC_TimeStruct = {0};   LL_RTC_DateTypeDef RTC_DateStruct = {0};   ...

EDuat.1 by Associate III
  • 2326 Views
  • 4 replies
  • 0 kudos

Resolved! How to update MCU package in CubeMX from download?

I am trying to update STM32CubeL4 package from v 1.14.0 to 1.16.0. Refreshing packages in manager does not show new versions. I downloaded zip from STM site and tried to add it using "From local" button. The integrity check and unpacking went withou...

maple by Associate II
  • 2300 Views
  • 3 replies
  • 0 kudos

Resolved! CAN and two UARTs in 20 pin TSSOP STM32F042?

Hello, can the pin configuration shown below possible?We need one bidirectional UART and a CAN along with a UART TX for debugging. Questions are:It says "Pin pair PA11/12 can be remapped in place of pin pair PA9/10 using the SYSCFG_CFGR1 register" So...

0693W000006FXukQAG.png
PNare by Associate III
  • 2784 Views
  • 5 replies
  • 0 kudos

Resolved! Most peripherals are inactivated in CubeMx.

Hi,I m working on STM32F769-DISCO board. I m using on STM32CubeIDE(vers. 1.5.0) and internally CubeMx(vers. 6.1.0). When I create new project, CubeMX interface is opening as you see on attached screen shot.I can not activate USB_OTG_FS as "Device Mod...

AK47 by Associate II
  • 2601 Views
  • 3 replies
  • 0 kudos

Resolved! Watchdog Feeding Issues with FreeRTOS

Hello All, Working with an STM32F4 processor and having issues with feeding the independent watchdog. Code is CubeMX generated. FreeRTOS v10.2.1 and CMSIS-RTOS V1.02. Watchdog resets if not fed every 512ms. Watchdog is fed in its own task and the pri...

Pain by Associate II
  • 4389 Views
  • 3 replies
  • 0 kudos

Resolved! stm32l4 64 pin and SDMMC 4 bits wide bus

Hello, I'm using an stm32l496rgt (64 pins).When I set SD 4 bits wide bus on SDMMC I noted that the code created set SDMMC_BUS_WIDE_1B instead of 4B.In this configuration the sd card doesn't work, it works only with 1 bit bus.4 bits data bus works pro...

0693W000006FFWVQA4.png 0693W000006FFWfQAO.png
DVacc.1 by Associate II
  • 2849 Views
  • 3 replies
  • 0 kudos