STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 2 kudos

Timers Interrupts NOT WORKING STM32F401RE

Hi guys!I'm trying to do a simple blinking led using interrupts but they never get fired.I'm using 84 MHz clock frequency and the following options:  /* USER CODE BEGIN Header */ /** *****************************************************************...

0693W000007B0mtQAC.png 0693W000007B0mUQAS.png
JCuer.2 by Associate II
  • 2354 Views
  • 2 replies
  • 0 kudos

I have compile issue with stm32cubemx.

Hello sir, CPU : stm32f407VGTI just set ETH and LWiP and generate file using stm32cubemx. The file is generate succefully. But the file has error with IAR version7.  ​=========================================================file name : mpu_armv7.h __...

Resolved! I2C NVIC function is not create

Hi,I tried to I2C Loopback test on STM32F401.I added two I2C Ports and checked NVIC Setting.Following some of tutorials, below function is craete automatically.but when i generated codes, this function was not crated.this function is wrote by user?

0693W000007AqSFQA0.png 0693W000007AqSKQA0.png

Resolved! STM32CubeMX 5.6.0 (latest) Code Generation Freezes

I'm trying to generate the code on the STM32F407G-DISC1 evaluation board for the TrueStudio project environment.The code generation just freezes.Has anyone else seen this?I'm running on Windows 7 Pro, 64 bitI've tried different combinations of projec...

0693W000000VReZQAW.png
SidBr by Associate II
  • 3613 Views
  • 8 replies
  • 0 kudos

Resolved! usart.h / usart.c and the gpio.h / gpio.c files are missing

I am using a Nucleo F091RC.When I create a new project, the .../Inc/usart.h .../Src/usart.c .../Inc/gpio.h.../Src/gpio.c files are missing.The button on the board is declared as GPIO_InputThe LED on the board is declared as GPIO_OutputPA2 is declar...

FLamb.2 by Associate II
  • 4285 Views
  • 1 replies
  • 1 kudos

STM32F103 TIM2 counting properly but won't interrupt

For a simple LED Blink program using interrupts, TIM2 is counting correctly, but its IRQs are not happening. As expected, there are about 1440 TIM2 "count-outs" per 1.0 seconds.Over the past few years several CubeMX timer IRQ bugs have surfaced, but ...

0693W000006HKb5QAG.png 0693W000006HKbKQAW.png
RPasc.2 by Associate III
  • 7981 Views
  • 16 replies
  • 0 kudos

Resolved! I am getting this error message "These IPs still have some not configured or wrong parameter values : [FATFS]" when trying to generate code on STM32CubeMX

Hii,While configuring STM32F446RE on CubeMX version 5.0.1 for using the board for reading and writing data on an SD card using SDIO mode (1 bit mode), after enabling this mode and then enabling SD Card option in the FATFS Middleware, it asks me to re...

SSoni by Associate III
  • 3669 Views
  • 4 replies
  • 1 kudos