STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

How to use DMA to update the PWM setting on a timer

Hi all,I am using a PWM timer. That is initialized and works fine.Code for init below:static void MX_TIM2_Init(void) {   /* USER CODE BEGIN TIM2_Init 0 */   /* USER CODE END TIM2_Init 0 */   TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TI...

SSchu.4 by Associate II
  • 1558 Views
  • 1 replies
  • 0 kudos

Resolved! What could cause Usb Bad Descriptor and how to debug

Hello, It's my first try with Usb directly on an MCU, i used stm32cube mx and code generator to make a first test but when i'm running a simple cdc code i get windows throwing me an error about usb bad descriptor.I linked my ioc and my usb schematic,...

0693W000006E90lQAC.png
FGERA.1 by Associate
  • 2457 Views
  • 5 replies
  • 0 kudos

Resolved! Migrating to new Cube version

Hi, some year ago i loaded STM32CubeIDE_1.2.0 and the package STM32Cube_FW_F4_V1.24.0 and i make some project (26). Now I load STM32Cube32 1.5.0 and package STM32Cube_FW_F4_V1.25.0.The packages are loaded in the same area (Repository).I try to import...

Evaluating the X-NUCLEO IHM16M1 board using STM32CubeIDE. Working add on package for CubeMX cannot be found.

I am attempting to evaluate the X-NUCLEO IHM16M1 board using STM32CubeIDE.  MCU board is a NucleoF401RE. I have tried to find a (working) add on package for CubeMX but can only find .zip files with example code for Kiel etc.  Is there an add on packa...

Why is there no way to export a CMSIS/HAL set from CubeMX?

The packs we can download contain entire STM32Fx series with include files for everything.When we select a specific MCU in CubeMX we should be able to use this to export a "clean" set of HAL and CMSIS files as well as potential low level boot/init f...

kyrreaa by Associate III
  • 2658 Views
  • 7 replies
  • 0 kudos

Resolved! Re-run STM32CubeMX after generating code ?

After creating a new project STM32CubeMX it automatically generates code. If I want to change any setting using STM32CubeMX how can it be restarted from within STM32CubeIDE ?I ran STM32CubeMX by double-clicking the .ioc file, but STM32CubeMX does no...

RPasc.2 by Associate III
  • 4447 Views
  • 6 replies
  • 0 kudos

SPI speed limited to 40 MHz on STM32L4R5Zi?

Hello! I was looking at the datasheet for the STM32L4R5ZI chip and it shows the limitation of the SPI (for the 2.7V to 3.6V range). I set this in the *.ioc file and tried to select a prescaler of 2 on a 120 MHz block to get a frequency of 60 MHz. ...

JayDev by Senior II
  • 2350 Views
  • 2 replies
  • 0 kudos