cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX-5.2.1 installation path

VPrib
Associate

STM32CubeMX-5.2.1 - why I can't install it in d:\STM32\STM32CubeMX path?

I use d:\STM\ for \STM32 ST-LINK Utility\ , \STMStudio\ and other STM application. Why not CubeMX?

Setup returns error: Invalid directory path. Please enter a directory path meets the operation system's requirements.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Miguel XRay
Associate II

Same problem to me, on Windows 10 (64 bit), no install directory will make it happy, I cannot install the software.

GokhanBektas
Associate

You need to use capitalized drive letter "D" instead of "d"

Then it should work fine.

Thanks a lot, it works.

This is a really stupid bug, but your answer is of great use!

NBlas.1
Associate

GokhanBektas thanks for the contribution please but sometimes capitalizing the drive letter doesn't work . When I faced the same problem, I only when into that directory/path and permanently deleted the folder STM32Cube, then when I continued with the installation, it went on successfully.