STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1583 Views
  • 0 replies
  • 2 kudos

NUCLEO-L476RG SDMMC problem

Hi everyone,I am starting using the STM32 to store data on MicroSD card over the SDMMC port. My board is a NUCLEO-L476RG. CubeIDE version is 1.6.1 and CubeMX is 6.2.1.My MicroSD card is a basic 2GB model, it works perfectly well when connected throug...

0693W00000AMQtzQAH.png 0693W00000AMQsyQAH.png 0693W00000AMQtkQAH.png 0693W00000AMQtVQAX.png
MSzab.2 by Associate
  • 1376 Views
  • 1 replies
  • 0 kudos

Resolved! FMC SDRAM Configuration

I am unable to configure FMC with SDRAM in latest STM32CubeIDE 1.6.1.Regardless of what I chose in the Mode section. Can someone guide me, what settings I have to perform?

0693W00000Bbk7BQAR.jpg
TRadd.1 by Associate II
  • 3124 Views
  • 5 replies
  • 0 kudos

Clock configuration using CubeIDE

Hi,i have a simple question: how do i have to configurate the clock of my STM32F072RB to send or receive CAN-Messages with 500kBit/s. With 8MHz it seems to work only until 250kBit/s.Best regards

NDorn.1 by Associate II
  • 3029 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F407 Virtual com port error 43

Hello, I use STM32F407 and I wanna config virtual com port on my board using CubeMX,but I always get error 43, I saw many topics, my stack size is 0x4000 and heap size is 0x2000.I tried to change max packet size, reinstall stm32 vcp drivers, but noth...

qqAnton by Senior
  • 2927 Views
  • 5 replies
  • 0 kudos

Resolved! CubeIDEMX doesnt' enable RCC bit?

I used STMCubeIDE to generate the following code...It is for Timer16 to count up and generate an interrupt after 100ms. Can someone tell me why the code did not set up __HAL_RCC_TIMx_CLK_ENABLE()?When I use the IDE to generate GPIO stuff it automat...

SWenn.1 by Senior III
  • 1318 Views
  • 2 replies
  • 0 kudos