User Activity

I am trying to import (STSW-SPIN3202-V1.0.0 ) to cube IDE. I get the following errors. Seem to be related to the linker config file. The paths are not correct. How do i fix this issue ? I used the "Import" from existing project and file import option...
STEVAL-SPIN3201After looking at the schematic i can see that there is a second MCU to 'control' the STSPIN32F0. This second MCU has a STLINK connector for programming. My question is ; Is it possible to program the STSPIN32F0 directly and not have to...
When i open an example project everything works OK. When i create a project using CUBEMX or the IDE i see a limited number of drivers. Working with STM32F411RE. I don't see any LL Drivers.