STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

LwIP DHCP request not working on STM32F7

Hi all,I am trying to get LwIP running on my STM32F769I-Discovery board. It works fine with the provided netconn-example.But when I try to generate a new project inside CubeIDE the dhcp-discovery is always failing. I can not see anything when running...

Resolved! Serial Wire debug problems

I'm working on a low power project using the Stm32f103 (blue pill) and I've been having problems, which I'm pretty sure are related to Serial wire debug , I am using a low frequency ( 256 pre-scaler) to save power on the HCLK , and every time I attem...

0693W00000D18TZQAZ.png 0693W00000D18RiQAJ.png 0693W00000D18ROQAZ.png
HAbay.1 by Associate III
  • 4097 Views
  • 2 replies
  • 0 kudos

How to update only HAL usart drivers in my program ?

I have used stm32cubemx v5.2 to create my project .Now i want to update only Uart drivers to drivers of cubemx V6.3 (latest drivers)How to do it ?Is it safe to just replace ?stm32l0xx_hal_uart.c and stm32l0xx_hal_uart.h with newer drivers ?

SA.17 by Associate III
  • 1563 Views
  • 2 replies
  • 0 kudos

CubeMX LwIP initial Ip problem

Hi, I kindly need your help. I have a STM32F769 and TCP server application . I am using LWIP stack . In my application server is arm and PC is client. When client tries to send something to arm, arm binds client’s ip address. So the connection is ok ...

nur by Associate II
  • 2080 Views
  • 4 replies
  • 0 kudos