User Activity

Hello everyone! I want to use a TCP/IP stack with my Nucleo STM32F207ZG over FreeRTOS, so I went ahead and created an stm32 project with STM32CubeIDE and initialized the project with cubeMX. (see linked file).So far so good! My problem begins when I ...
Hello,So I bought a B-L4S5I-IOT01A with the intention to use it as a MQTT device to send and receive data. My problem is that i cannot communicate with the on board Wi-Fi chip "STM32_IWIN_WIFI_V2". Here's what I did :1- I create a project with STM32C...
Hello everyone, I am currently working on a project with touchGFX (4.13.0) and I want to use CMSISv2 functions and calls. Since the default configuration from touchGFX is CMSISv1, I open the cubeMX project created by touchGFX and changed the CMSIS ve...
Kudos from