2021-01-14 10:28 AM
Hello everyone!
I want to use a TCP/IP stack with my Nucleo STM32F207ZG over FreeRTOS, so I went ahead and created an stm32 project with STM32CubeIDE and initialized the project with cubeMX. (see linked file).
So far so good! My problem begins when I try to read incoming packets, I use the function lwip_read() (alose tried read()) to read from the input buffer sequentially. It works a couple of times then the thread crashes. see code snipet below :
Code
So I have a single thread, that I pasted below. In it I use an MQTT library. All the function I use from this library only write to CHAR buffers and do not interact with the TCP/IP Stack.
The code here is simple and it's purpose is to demonstrate read and write capabilities to the network. The code crashes at line 70. I don't know why. (I know that it's weird to have a couple of read like that, but it is only to better show the symptoms of the problem).
void StartDefaultTask(void *argument)
{
/* init code for LWIP */
MX_LWIP_Init();
/* USER CODE BEGIN StartDefaultTask */
// Init variables and constants
MQTTPacket_connectData data = MQTTPacket_connectData_initializer;
char buf[200];
int buflen = sizeof(buf);
MQTTString topicString = MQTTString_initializer;
char* payload = "76";
int payloadlen = strlen(payload);
int len = 0;
int port = 1883;
int sock = 0;
struct sockaddr_in serv_addr;
char *ip = "192.168.0.139";
uint8_t toSend[50] = {0};
int sendStatus = 0;
int receiveStatus = 0;
int errorbuffer = 0;
int psi = 0;
/* Infinite loop */
for(;;)
{
// Create socket
if ((sock = socket(AF_INET, SOCK_STREAM, 0)) < 0)
{
printf("\n Socket creation error \n");
}
// Convert IPv4 and IPv6 addresses from text to binary form
serv_addr.sin_family = AF_INET;
serv_addr.sin_port = htons(port);
if(inet_pton(AF_INET, ip, &serv_addr.sin_addr)<=0)
{
printf("\nInvalid address/ Address not supported \n");
}
// Connect to server
if (connect(sock, (struct sockaddr *)&serv_addr, sizeof(serv_addr)) < 0)
{
printf("\nConnection Failed \n");
}
// Create MQTT Message
data.clientID.cstring = "1";
data.keepAliveInterval = 10000;
data.cleansession = 1;
data.username.cstring = "testuser";
data.password.cstring = "testpassword";
data.MQTTVersion = 4;
len = MQTTSerialize_connect((unsigned char *)buf, buflen, &data);
// Send mqtt message
sendStatus = send(sock, (char*)buf, len, 0);
if( sendStatus < 0){
errorbuffer = errno;
snprintf((char *)toSend,sizeof(toSend),"\r\nReturn status of send : %d, %d\r\n", sendStatus, errorbuffer);
HAL_UART_Transmit(&huart3,toSend,strlen((char *)toSend),10);
}
// Receive CONNACK
receiveStatus = lwip_read(sock,(char*)buf, 1);
receiveStatus = lwip_read(sock,(char*)buf + 1, 1);
receiveStatus = lwip_read(sock,(char*)buf + 2, 1);
receiveStatus = lwip_read(sock,(char*)buf + 3, 1);
//<!><!><!> CRASHES HERE <!><!><!>
receiveStatus = lwip_read(sock,(char*)buf + 4, 1);
receiveStatus = lwip_read(sock,(char*)buf + 5, 1);
receiveStatus = lwip_read(sock,(char*)buf + 6, 1);
receiveStatus = lwip_read(sock,(char*)buf + 7, 1);
if (MQTTPacket_read((unsigned char*)buf, buflen, lwip_read) == CONNACK)
{
unsigned char sessionPresent, connack_rc;
if (MQTTDeserialize_connack(&sessionPresent, &connack_rc, (unsigned char *) buf, buflen) != 1 || connack_rc != 0)
{
printf("Unable to connect, return code %d\n", connack_rc);
}
// print connection result
snprintf((char *)toSend,sizeof(toSend),"\r\nConnexion Success with code: %s, %s\r\n", sessionPresent, connack_rc);
HAL_UART_Transmit(&huart3,toSend,strlen((char *)toSend),10);
}
close(sock);
osDelay(1000);
}What am I doing wrong ? Any help is welcome !
Alexandre,
Thank you and have a great day!