2021-07-21 6:05 AM
Hi,
my STM32L151RC-A running at 65,536 khz with the MSI.
I´ve created the basic code with STMCubeMX.
i´ve tried to use this command to use the low power run mode:
HAL_PWREx_EnableLowPowerRunMode();
But this does nothing :\
Same power comsumption at 168µA (ST-Link is dissconnectet when i measure the Current.)
The standby mode works fine with a comsumption at 2µA.
Does anybody have an idea why i cant switch the low power run mode?
Main.c source:
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2021 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
/* USER CODE BEGIN 2 */
//HAL_SuspendTick();
HAL_PWREx_EnableLowPowerRunMode();
/* Enter LP RUN mode */
/* Wait until the system enters LP RUN and the Regulator is in LP mode */
while(__HAL_PWR_GET_FLAG(PWR_FLAG_REGLP) == RESET)
{
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_12); /*LED PORT 2*/
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_13); /*LED PORT 1*/
HAL_Delay(50);
}
//enter_LPRun();
//SET_BIT(PWR->CR, PWR_CR_LPSDSR);
//SET_BIT(PWR->CR, PWR_CR_LPRUN);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_Delay(5000);
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_12); /*LED PORT 2*/
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_13); /*LED PORT 1*/
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = 0;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_0;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12|GPIO_PIN_13, GPIO_PIN_RESET);
/*Configure GPIO pins : PB12 PB13 */
GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
2021-07-21 9:39 AM
Maybe you need other code this is from example LPRUN
while (1)
{
/* Configure User push-button*/
BSP_PB_Init(BUTTON_KEY,BUTTON_MODE_GPIO);
/* Wait Until User push-button pressed */
while(BSP_PB_GetState(BUTTON_KEY) != GPIO_PIN_RESET)
{
}
/* Wait Until User push-button released */
while(BSP_PB_GetState(BUTTON_KEY) != GPIO_PIN_SET)
{
}
/* Enter LP RUN mode */
HAL_PWREx_EnableLowPowerRunMode();
/* Wait until the system enters LP RUN and the Regulator is in LP mode */
while(__HAL_PWR_GET_FLAG(PWR_FLAG_REGLP) == RESET)
{
}
/* Wait Until User push-button pressed */
while(BSP_PB_GetState(BUTTON_KEY) != GPIO_PIN_RESET)
{
}
/* Wait Until User push-button released */
while(BSP_PB_GetState(BUTTON_KEY) != GPIO_PIN_SET)
{
}
/* Exit LP RUN mode */
HAL_PWREx_DisableLowPowerRunMode();
/* Wait until the system exits LP RUN and the Regulator is in main mode */
while(__HAL_PWR_GET_FLAG(PWR_FLAG_REGLP) != RESET)
{
}
}Remark this code is from L0 fw,