STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1557 Views
  • 0 replies
  • 2 kudos

The project description file (.project) is missing.

Hi,Code is generated using CubeMX, the attached screenshots may demonstrate the issue:CubeMX v 6.3.0CubeIDE v 1.8.0TouchGFX 4.18.0_M7Why 2 projrcts are created, one for CM4 and another for CM7?Thank you in advance for your help

0693W00000KZmI8QAL.jpg 0693W00000KZmHAQA1.jpg 0693W00000KZmGlQAL.jpg 0693W00000KZmGWQA1.jpg
ksale.1 by Senior II
  • 4712 Views
  • 8 replies
  • 0 kudos

STM32F429ZI - Nucleo I am trying to setup a Master - slave configuration where TIM2 is in encoder mode being the master TIM1 is in One pulse mode being the slave. I am wondering what should the "Trigger Event Selection" on TIM2 should be

I would like the Trigger Event of TIM2 to be generated when the Encoder count reach a specific position. #include "main.h"   TIM_HandleTypeDef htim1; TIM_HandleTypeDef htim2;   UART_HandleTypeDef huart3;   void SystemClock_Config(void); static void M...

0693W00000Kb1XoQAJ.png 0693W00000Kb1aFQAR.png 0693W00000Kb1dmQAB.png
DPatr.2 by Associate III
  • 1592 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G030C8t6 pin conflict!

hey there,I have a STM32G030C8t6 which I wish to configure. in CubeMX when I focus on PA11 or PA12, I can see a bracket where this is mentioned:PA11[PA9]PA12[PA10]what does it mean? does it mean they are somehow connected or related? can anyone expla...

Ala by Senior
  • 1689 Views
  • 3 replies
  • 0 kudos

stm32h750 and lan8720

hi i have a custom pcb with lan8720 chip on it and i can't access or ping it also cubeMX doesnt support lan8720 it only support 8742 please help i'm using cubeIDE and cubeMX

bakhti by Associate II
  • 1018 Views
  • 0 replies
  • 0 kudos

Resolved! Is there mistake in datasheet?

My fellow student says TIM12 has 2 channels and PH9 is configured for TIM12 channel 2 as per the below datasheet.https://www.st.com/resource/en/datasheet/stm32h743vi.pdfNow I argue that the tim12 channel 2 is configured to PB15.And he stupidly config...

0693W00000KZyjpQAD.png
Vmere.1 by Senior
  • 1456 Views
  • 3 replies
  • 0 kudos

no UART console output for STM32F429ZI dev-kit

I have no console output for UART;I am using STM32F429ZI dev-kit CubeMX and STM32CubeIDEThe codes compiles and I can see the light blinking but when I connect to Serial terminal with PuttY, I observe no console output.What am I missing ?/* USER CODE ...

0693W00000KaRmOQAV.png
DPatr.2 by Associate III
  • 6115 Views
  • 10 replies
  • 0 kudos