Good starting point for VCP module (FT232 replacement)
I just ordered a PCBA with FT232RL as USB-VCP bridge and found that these things are bulky, expensive and out of stock mostly.
So why not design a USB-serial (eg. 3.3 V 9600 bd) bridge using any STM32?
I am aware that CubeMX supports USB/VCP so this is a starting point already. However, to save time and effort, are there any existing projects that implement a VCP - serial bridge already? Ideally with baud rate selectable on the host (Windows 10)? Even better with working CubeMX integration (unlike most existing STM32 example programs) and CubeIDE project?
No preference on family, any F1 or F0 would probably do. Maybe one with Nucleo32 (64) support.
Thanks - Martin