Skip to main content
Mmohs.1
Associate
July 28, 2021
Question

How can we run the program generated by STM32CubeMX without having to use the GUI?

  • July 28, 2021
  • 3 replies
  • 1013 views

..

This topic has been closed for replies.

3 replies

TDK
July 28, 2021

You need to compile it with an IDE such as STM32CubeIDE, then upload it to the chip using the IDE or STM32CubeProgrammer.

You also need to add your own code to make the program do something useful.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Mmohs.1
Mmohs.1Author
Associate
July 28, 2021
What file(s) need to be uploaded to the chip? We used STM32CubeIDE to build the application, but we want a simple way to load & run the application without having to start up the IDE and click on buttons.
TDK
July 29, 2021
The *.ELF file needs uploaded which is in the build directory (typically Release or Debug). Sometimes the ELF is converted to a HEX or BIN which, for this purpose, are equivalent.
It can also be uploaded with the STM32CubeProgrammer command line interface.
"If you feel a post has answered your question, please click ""Accept as Solution""."