cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 6.3.0 BUG?

tsuna
Associate II

main.c generated by STM32CubeMX 6.3.0

Line 23

#include "usb_device.h"

#include "usb_device.h" Are duplicated.

Then MX_RTC_Init () is missing HAL_RTCEx_SetWakeUpTimer_IT ().

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hello @tsuna​,

Thanks for having reported.

You're right, I've been able to reproduce the issue. I assume the duplication of #include "usb_device.h" is due to the activation of both USB and FreeRTOS middleware.

This misbehavior will be reported internally to be fixed. I'll keep you posted with the updates.

Sorry for any inconvenience that this may cause.

Meanwhile, trying with the previous STM32CubeMX version 6.2.1, the issue doesn't occur:

  • #include "usb_device.h" is generated just once.
  • HAL_RTCEx_SetWakeUpTimer_IT () is correctly generated in MX_RTC_Init () .

Khouloud.

View solution in original post

1 REPLY 1

Hello @tsuna​,

Thanks for having reported.

You're right, I've been able to reproduce the issue. I assume the duplication of #include "usb_device.h" is due to the activation of both USB and FreeRTOS middleware.

This misbehavior will be reported internally to be fixed. I'll keep you posted with the updates.

Sorry for any inconvenience that this may cause.

Meanwhile, trying with the previous STM32CubeMX version 6.2.1, the issue doesn't occur:

  • #include "usb_device.h" is generated just once.
  • HAL_RTCEx_SetWakeUpTimer_IT () is correctly generated in MX_RTC_Init () .

Khouloud.